7/8/2023 1:47 PM | |
Joined: 12/11/2019 Last visit: 8/6/2024 Posts: 1 Rating: (0) |
I have a problem with the controller with the process heating wire, I have a machine using SIVOLT as controller, it is used as a voltage regulator for the process annealing of the wire, because SIVOLT is out of production and looks like it can be replaced using Sinamics DCM, but I am confused with the wiring diagram for the setpoint and parameters that have been changed and if using an external power module how to connect the cable from the DCM controller to the power module and what is needed if using a Power unit topology 2: 6-conductor connection (open delta connection) https://support.industry.siemens.com/cs/id/en/view/109763610 Thank You |
Last edited by: Jen_Moderator at: 07/10/2023 11:03:37Link optimized. |
|
Follow us on