1/21/2022 8:49 PM | |
Joined: 10/17/2007 Last visit: 7/14/2024 Posts: 4008 Rating:
|
I see you have big trouble , No one can help you only by yourself. Remember the 1st time I answered you--the meaning is Do Not replace NCU with different type. if you doing it that you have your risk . I response for you just though if you are lucky to fix the machine in time. but now coming to the reason why you HAVE to use NCU572.4 to replace NCU572.5. Time IS money go to online market to find a used NCU572.5 . I attached a link FYI another tips for you SIMATIC Manger #1--you only post many pictures of your PC/PG screen shoots for S7 project and so on No any picture (to show me ) of NCU front --I need to see LED's and will know Why cannot you go online.---Attention I saw you have in HMI alarm "Waiting to connect NCU" --that mean you cannot go communication to you NCU to HMI, of course no communication to PLC as well. --I guess you have PF and PS red led's flash on the NCU--in this situation don't try to go online #2--You have so many trouble due to change NCU type, which are no worth to discussion. But I want to remind you, If you PC/PG is standard SIMATIC manager --FOR Standard along PLC . You will have trouble to make back up (HW configuration) when you connecting to PLC integrated inside NCU572.x . YOU NEED to install "840D Toolbox" --which has add on "SW" for the SINUMERIK
AttachmentNCU_link.docx (272 Downloads) |
Last edited by: nulizhang at: 01/21/2022 20:54:29Last edited by: nulizhang at: 01/21/2022 21:00:18attached link If you like my comments please |
|
Follow us on