10/7/2013 11:48 AM | |
Posts: 3609 Rating:
|
Import of a Technical Question of the User SIS AN
|
10/7/2013 4:11 PM | |
Joined: 9/27/2006 Last visit: 8/14/2024 Posts: 12277 Rating:
|
Hello SIS AN;a psb file is a Prosave backup. Ypou can only restore this file on a panel witht he same part number as the original one. See this link: I have taken Back up from the TP270 in the form of *.psb.How to restore this file on to MP Panels? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/7/2013 4:11 PM |
|
10/9/2013 3:29 PM | |
Joined: 4/29/2010 Last visit: 8/12/2024 Posts: 1557 Rating:
|
This isn´t correct. The part number isn´t necessary in this case, it´s the type of the panel wich is necessary. Working example: For example if you have a backup of a OP17/DP: 6AV3 617-1JC20-0AX1, you can restore this backup without any problem to a OP17/DP: 6AV3 617-1JC20-0AX2. The type of the panel must be the same but not the part number (OP17/DP <equal> OP17/DP). Not working example: For example if you have a backup of a OP17/DP: 6AV3 617-1JC20-0AX1, you can´t restore this backup to a OP17/DP-12: 6AV3 617-1JC30-0AX1. The type of the panel are not the same (OP7/DP <unequal> OP7/DP-12) With best regards |
This contribution was helpful to
2 thankful Users |
11/26/2013 8:39 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
There is nothing with memory. But if Siemens tried there...I don't know. Best regards, Hristo Mihalev
|
Follow us on