Industry Online Support
Technical Forum
2/19/2008 2:33 PM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating: (8) |
Dear, there is no special guideline to tranfer parameters from FC(CU1) plus T100 to CUVC. Most of the T100 functions are implemented in the free-functions-blocks of CUVC. So analzye the T100 function in our application and "transfer" it to the CUVC. It needs a complete new start-up. This may help: http://support.automation.siemens.com/WW/view/en/13472409 This for CU2 ==> CUVC, but basically useful fo rCU1, too http://support.automation.siemens.com/WW/view/en/22642090 |
2/20/2008 5:31 AM | |
Posts: 2 Rating: (0) |
Thanks for help. |
Follow us on