Industry Online Support
Technical Forum
4/11/2011 10:49 AM | |
Posts: 4 Rating: (0) |
Hi I have the same problem with connections on the same card, 6ES7 334-0KE00-0AB0, but I have a 3 wire pt100 to connect to channel 0. Will the connections be the same as per this diagram white = 2 red = 3 red = 4 Is this correct? Is there anything elst that needs to be done with connection Mana? Your assistance would be greatly appresiated Thank you Splitted from Request 4 wire pt 100 wiring connection to SM334. |
Last edited by: O_Moderator at: 4/12/2011 10:22 AMnew subject after splitting |
|
4/11/2011 4:10 PM | |
Posts: 23 Rating: (0) |
Hello Marcjan, Thanks for your techincal suggestion. I will change as per you suggestion and will let you know if OK. Again thanks. |
4/14/2011 5:08 PM | |
Posts: 4 Rating: (0) |
Hi Marcjan Thank you for the advice, but it didn't work for me, the output was full scale on this connection, however, I have attached the drawing of the connections as they are now and it woks The only problem is that the 2 output from this card stopped working, so I might have destroyed the card from all the different connections I tried. There doesn't seem to be accurate information from Siemens on how to connect devices/components to their cards Anyway, thanks again for the time // Baie Dankie Regards Arno PS sorry for the size of the .pdf AttachmentPT100 Connection.pdf (445 Downloads) |
Last edited by: Arno_H at: 4/14/2011 5:08 PM |
|
Follow us on