12/17/2016 3:19 PM | |
Joined: 9/27/2006 Last visit: 9/4/2024 Posts: 12282 Rating: (2682)
|
Hello Balakrishnan; Your point is correct. To enable a S7-414-5H CPU as a F-CPU you need an extension, S7 F-Systems. The latest version is S7-Systems v6.2 (license numbers are available in the second link below): you also need a S7F-systems RT license. SIMATIC Industrial software S7 F/FH Systems - Configuring and Programming https://support.industry.siemens.com/cs/ww/en/view/109742100 S7 F/FH Systems fail-safe systems The fail-safe automation systems ("F-Systems") S7 F/FH Systems are used in systems with stringent safety requirements. The objective of S7 F/FH Systems is to control processes with an immediately achievable safe state. In other words, F-Systems control processes in which an immediate shutdown does not endanger people or the environment. The S7 F Systems optional package comprises the following two components: ● S7 F Configuration Pack V5.5 SP6 ● S7 F Systems V6.1 S7 F Systems V6.2 Released for Delivery https://support.industry.siemens.com/cs/ww/en/view/109740650 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/17/2016 4:56:19 PM |
|
This contribution was helpful to2 thankful Users |
Follow us on