7/31/2006 9:20 AM | |
Joined: 4/24/2006 Last visit: 8/9/2024 Posts: 8713 Rating:
|
Hi Pandiani, Which S5-CPU are you using? Best regards, Wizard |
7/31/2006 8:21 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
[quote user="Pandiani"]Can anyone explain or suggest link with informations about resetting S5 PLC processor. I need to know how to reset it, and what "overall" reset means and how to perform it. Hi Pandiani, Please look in any handbook from a PLC.... [:)] S5-90U/S5-95U Programmable Controller System Manual S5-100U Programmable Controller S5-115U Programmable Controller S5-115U Programmable Controller CPU 945-7UA1./-7UA2. S5-135U CPU 928B - Version -3UB21 SIMATIC S5-135U/155U System Manual Those S5 CPUs are only a few one, but the most sold are between it... [;)] When the one that you search for is not between those, please look on the SIMATIC SUPPORT and type in the PLC type in the right up corner, for example "95u" and choose on the left only for the handbooks "Only manuals/operating instructions", there you might find every handbook that is from this age... [8)] "overall reset" means that you bring back the CPU to his initial state. When you want to try something, please first make a backup.. [:blush:] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
8/1/2006 9:26 AM | |
Joined: 10/31/2005 Last visit: 8/6/2024 Posts: 366 Rating:
|
Thanks for valuable informations. |
Follow us on