5/4/2011 3:17 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359) |
FB41 and FB50 called in OB35.There is also a sample project here to check the possible configuration. PID Self Tuner: Example Adapted to Standard PID Control V5.1
Check the selected sections of the following manual: System Software for S7-300/400 System and Standard Functions Volume 1 and Volume 2 1- 29.3 Controlling the Counter with SFB 47 "COUNT" 2- 29.4 Controlling the Frequency Measurement with SFB 48 "FREQUENC" regards |
5/5/2011 4:21 AM | |
Posts: 6 Rating: (0) |
Thank you so much. have you a nice day. |
This contribution was helpful to1 thankful Users |
5/5/2011 5:16 AM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359) |
Also check the manual of the product here for more information: PID Self-Tuner V5 regards |
Follow us on