2/9/2012 10:08 PM | |
Joined: 2/6/2012 Last visit: 1/30/2023 Posts: 46 Rating:
|
Hello i just try to redo the same function as i did with a previous v10.5 projet and have a Tonr to count trigger on count done reset timer when i try to program de ''RT'' fonction, it doesn't accept my timer adress or any other timer adress Is there anything new that i've missed ? I've look in the help file but it doesn't tell how to resetori redo the same as the help for RT andmy RT tag style remain un red... I did compile the whole project in case the timer DB has to be compiled first butremain the same... any helpwould be appreciated Attachmenttimer.pdf (101 Downloads) |
2/13/2012 5:28 PM | |
Joined: 2/6/2012 Last visit: 1/30/2023 Posts: 46 Rating:
|
when not working
Attachmenterror1.pdf (89 Downloads) |
2/13/2012 5:28 PM | |
Joined: 2/6/2012 Last visit: 1/30/2023 Posts: 46 Rating:
|
working
Attachmenterror1_OK.pdf (94 Downloads) |
2/13/2012 5:40 PM | |
Joined: 2/6/2012 Last visit: 1/30/2023 Posts: 46 Rating:
|
DTL issue AttachmentBureau.zip (84 Downloads) |
Follow us on