11/2/2021 9:19 PM | |
Joined: 2/28/2021 Last visit: 5/4/2024 Posts: 5 Rating: (0) |
On my SFC faceplate, the restart and the reset button are missing. Any solution how I can enable those buttons? I have attached below a picture of my SFC faceplate. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/03/2021 09:14:25New subject after splitting |
|
11/4/2021 7:12 AM | |
Joined: 1/11/2019 Last visit: 4/30/2024 Posts: 702 Rating: (140) |
Hi MA08, You can enable the Restart button in the faceplate for the SFC and SFC type by following method. Open the graphic designer in WinCC -> navigate and open the below 2 .pdls 1. @pg_@sfc_rts_head.pdl (This .pdl is for SFC Types/Instances) 2. @pg_@sfc_type_head.pdl (This .pdl is for SFC) Double click on faceplate of above .pdls in graphic designer and Enables the restart radio button. (See the attached screenshot) Once you are done with above steps, kindly save the faceplate and Exit runtime and restart WinCC runtime. Also note the SFC assignments: Restart in the "Held / Held (Error)" state ENSTART = 1 and ENRESTART = 1 must be set to be able to restart in the "Held / Held (Error)" state. You can find additional information about multiple simultaneously pending commands in the sections: • Behavior when multiple commands are queued (Page 252) • Continuous mode (Page 241) PCS 7 SFC for SIMATIC S7 (V9.0 SP5) You can use the below link to know more about SFC Visualization (You can use the "SFC Visualization" software package to configure SFC visualization in WinCC and to perform operator control and monitoring of SFCs and SFC instances in the WinCC runtime system.) PCS 7 SFC Visualization (V9.0 SP5) Hope it helps you! |
This contribution was helpful to1 thankful Users |
Follow us on