6/15/2011 8:56 PM | |
Joined: 9/18/2006 Last visit: 5/29/2023 Posts: 586 Rating:
|
Hi. Do not worry. All fixable. The system is stored on the CF card. You destroyed the system. There are several solutions: 1) Refer to regional Siemens-representation. 2) Overwrite system CF-card inside 802D SL, writing the file there (copied from a working 802D SL system). Artorizatsiya lost, you recover it through the Internet: http://www.siemens.com/automation/license. I do not do it, but I think as an engineer, it should work. Best regards. |
Last edited by: pfuser at: 6/15/2011 10:28 PMOverwrite the image CF-card |
|
6/16/2011 6:54 AM | |
Posts: 67 Rating:
|
Thanks for your answer. I have no other 802D sl then I will call SIEMENS. Do you think updating system will reset the system ? |
6/16/2011 8:07 AM | |
Posts: 2964 Rating:
|
Hello.... Updating the system software will make default data....NC needs to be re-commissionied. Regards, Ekalavya |
6/16/2011 9:27 AM | |
Posts: 2964 Rating:
|
Hello, Check this link for the update.... /tf/WW/en/Posts/57569#top You can also make default from the main screen...i.e when booting you need to make select button ... Service menu will appear in this you have Default data option.... Hope you should have NC and PLC projects for running your axis.... Check it out.... Regards, Ekalavya |
6/16/2011 10:14 AM | |
Posts: 2964 Rating:
|
Hello... You will get this software from Siemens Only... Regards, Ekalavya |
Follow us on