6/13/2023 12:05 PM | |
Joined: 7/19/2022 Last visit: 7/17/2024 Posts: 376 Rating: (61) |
Hello walter_g, The KTP screensaver is deactivated when the user clicks on the screen or moves the mouse, if one is connected, but I don't know if it can be deactivated if some other event occurs, such as an alarm. Also, since the basic ones don't support scripts, you can't do much more. |
If this Information really helps, you could use the Rate function |
|
6/23/2023 9:39 AM | |
Joined: 7/5/2006 Last visit: 7/15/2024 Posts: 177 Rating: (4) |
Hello, with the comfort panel, it's work good. next days i will try with the basic panel. Thanks a lot |
Follow us on