6/26/2023 4:49 AM | |
Joined: 3/11/2019 Last visit: 7/5/2024 Posts: 1505 Rating: (270) |
Hi, at first, please check the firmware preconditions stated in the FAQ at the end of this mail. Please post the complete diagnostics buffer of the cpu as txt file after restart (if retentive data were lost, there must be entries). Please also post a screenshot of the correct hw config (configured like in FAQ). How do you use the complete data range of an S7-1500 V2.1.0 and higher as retentive memory with a system power supply PS 60W 24/48/60V DC HF?regards sancruz |
Feedback appreciated, please rate |
|
Follow us on