4/14/2018 2:58 PM | |
Joined: 12/18/2014 Last visit: 8/14/2024 Posts: 33557 Rating:
|
I once dared to realize a program for your case. As I wrote before, I do not have an HMI to do a real test. My test was with the web server and that's how it works. The test was with a 0BA8.Standard, I have no FS04 (or 05 or06). In the hardware selection there is a FS4 selected. AttachmentStoring_Setpoint_from_HMI_Fail-safe_in_LOGO!_(automatically)_FS4.zip (162 Downloads) |
This contribution was helpful to
1 thankful Users |
4/14/2018 4:37 PM | |
Posts: 171 Rating:
|
I solved it by using a Max/Min block. |
4/14/2018 4:40 PM | |
Posts: 171 Rating:
|
am not familiar with block diagram. but anyhow Max/Min is the only way i think. thankyou |
4/14/2018 5:00 PM | |
Joined: 12/18/2014 Last visit: 8/14/2024 Posts: 33557 Rating:
|
Here's in LAD.
AttachmentStoring_Setpoint_from_HMI_Fail-safe_in_LOGO!_(automatically)_FS4_LAD.zip (152 Downloads) |
This contribution was helpful to
1 thankful Users |
4/17/2018 9:26 AM | |
Posts: 171 Rating:
|
yes of course....but in this logic we cant set it to 0.. right? |
Follow us on