Industry Online Support
Technical Forum
2/18/2013 12:36 PM | |
Posts: 3609 Rating: (29) |
Import of a technical question of AmitC
|
2/18/2013 1:05 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Hello , You mean how to enable "retentivity" for a memory area? Also check: S7-1200 RETAIN MEMORY....Best regards Hamid Hosseini |
4/4/2013 10:47 AM | |
Posts: 22 Rating: (0) |
Dear Sir, I want to enable the retentive memory for particular register |
4/4/2013 11:27 AM | |
Posts: 461 Rating: (29) |
Hi, If u want a specific registry of data's to be retentive then create a DB with standard compatible with 300/400 so that the respective data's in that registry will be retentive if u enable rentivity. if ur creating a db with optimized then the retentivity can be defined by user.. Hope it helps Regards, Nelliyan.G AttachmentRetentivity.pdf (646 Downloads) |
Last edited by: Nelliyan randy at: 4/4/2013 11:28 AM |
|
7/23/2013 8:00 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Follow-up-question splitted to is it possible to add retentive memory using external memory card or is there any other way to increase retentive memory?. Best regards O_Moderator |
Follow us on