9/12/2019 11:13 AM | |
Joined: 10/4/2017 Last visit: 3/30/2024 Posts: 4 Rating: (0) |
Hi all, Despite reading lots of threads regarding problems with Reset blocks I have not been able to fix the problem I have. I have the following simple setup...
I get the classic 16#E7FE_0800 (Time out) error when trying to execute the Reset block. I have tried all different types of blocks, e.g. Reset_Reader, Reset_RF300 etc. I have also tried all different reader settings in the TO setup, e.g. RF300 general, RF300, Gen2 general, RF380R, Gen2 etc. The RF380R, Gen2 has a constant Blue LED The RF180C, ERR_1 and ERR_2 LED's blink very shortly every ~3 sec. I kindly ask for your help to solve this problem. Please see screen captures for further details. AttachmentCapture.zip (354 Downloads) |
9/12/2019 6:16 PM | |
Joined: 10/4/2017 Last visit: 3/30/2024 Posts: 4 Rating: (0) |
Magic! Thanks for your swift response Owei. With the I/Q for RF180C modified, using Reset_Reader block and TO's Reader-parameter assignment set to RF380R, Gen2, I am now able to reset the RF380R (now showing green LED). It did not occur to me to modify the I/Q settings since they were automatically assigned by TIA Portal. However, the celebrations are short lived. The Read and Write blocks both result in error code 16#E7FE_0400. The description of the error code does not make much sence to me since I am using TO and not getting involved in the inner working of the Ident profile etc. Are you able to shed light on possible causes/remedies of this particular error? Best regards, AttachmentCapture_E7EF_0400_02.zip (411 Downloads) |
9/13/2019 5:47 PM | |
Joined: 10/1/2013 Last visit: 5/2/2024 Posts: 605 Rating: (71)
|
I'm glad to hear it works. You're welcome. |
Follow us on