4/6/2018 4:58 PM | |
Posts: 167 Rating:
|
I have build up two fiber rings with Scalance XC206-2. Ring 1 = 26 switches I have no errors and everything is green in TIA portal. Network is stable and good, but when I try to make a fiber problem by disconnect a fiber cable the problems starts.... I have tried to ping all the ip addresses on ring 2... and when I make a error, I cannot see any differences on the ping response.... From documentation the MRP shall quantity max 200ms down time if you have less then 50 switches or something ? What can the problem be? Attachmentpicture.zip (441 Downloads) |
Last edited by: AutoGen_7361160 at: 4/6/2018 4:59:11 PM |
|
12/19/2019 11:54 AM | |
Joined: 8/21/2013 Last visit: 10/19/2024 Posts: 16 Rating:
|
Does anyone know how to solve this, I have the same problem. Thanks |
Follow us on