6/28/2010 7:56 AM | |
Joined: 6/3/2009 Last visit: 4/7/2025 Posts: 101 Rating:
|
Dear forum Members Ineed ring nework for my project(it 8 Port Switch). SCALANCE X104-2 (4-Port) 6GK5104-2BB00-2AA3 will support ring network and 6GK5108-0BA00-2AA3 is SCALANCE X108 (8-Port) wheather it will support ring network. So i can order the same. If i am worng give me MLFBno. formin. 8-Port with ring network should supportable. Help me........... |
6/28/2010 9:20 AM | |||||
Joined: 10/20/2009 Last visit: 4/3/2017 Posts: 215 Rating:
|
Dear WinCC, By using Scalance x104-2 & x108, you can form the ring but you cannot mange the ring as Ring Manager feature is not available with this X100 series. I suggest you go for X200 or X300 series. where you can also able to manage the ring. you can check following Scalances:
As per your application requirement. |
||||
Regards, |
|||||
6/28/2010 10:40 AM | |
Joined: 6/3/2009 Last visit: 4/7/2025 Posts: 101 Rating:
|
Dear R J Thanks for reply, i got it. |
Follow us on