6/2/2010 1:05 PM | |
Posts: 147 Rating: (34) |
Extending the answer a little:
Local data: Temporary data of a code block (OB, FB, FC) is saved to this memory area while the block is being processed. L1.0 means bit 0 of byte 1 (beginning from 0). It is valid only as long as the block is running, otherwise it does not exist. Since you are new, you can check this thread: ALL SIMATC Useful Manuals (Good for beginners on this Forum) The info above is in #10 (S7-300 CPU 31xC and CPU 31x: Technical specifications) Hope this helps. |
This contribution was helpful to2 thankful Users |
Follow us on