2/4/2014 11:01 PM | |
Joined: 3/6/2012 Last visit: 2/5/2025 Posts: 155 Rating:
|
Please find the communication manual in the link below Section 6.7 talks about the GSD files. Note: The Profibusmaster must be configured to have the same quantity of Bytes that are set by the parameter ‘Network I/O Size’ (9951) to communicate with the Siemens NXG drive. AttachmentNXG_Communications_manual_A5E02924901A_ver_AA.pdf (2254 Downloads) |
Last edited by: GrasserF at: 2/5/2014 7:54 AMAttachment edit www.chbdrives.com |
|
2/6/2014 12:07 PM | |
Posts: 2 Rating:
|
Thank you very much. I think it's gonna help me. |
3/11/2014 12:27 PM | |
Posts: 241 Rating:
|
have u found GSD?? if yes pls send here
|
4/11/2014 5:15 AM | |
Joined: 6/6/2011 Last visit: 11/15/2023 Posts: 8 Rating:
|
This is the only one I have, it has always worked for me.
AttachmentC:\Data\Manuals\ROBICON\Perfect harmony\NXG Communications\Profibus\Robi0868.zip (1359 Downloads) |
This contribution was helpful to
1 thankful Users |
10/9/2017 11:35 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by flex'y is split to a separate thread with the subject How received "profibus from drive" data must be scaled at PLC?. Best regards |
Follow us on