7/4/2009 7:58 AM | |
Posts: 18 Rating:
|
For diameter computation, you need to use a technology module T400 along with 6RA70.The appropriate software to be used along with T 400 is "Axial Winder". It is very difficult to compute diameter using S00 option of 6RA70. Kris AttachmentT400_Description.pdf (371 Downloads) |
7/4/2009 9:10 AM | |
Posts: 160 Rating:
|
Apart from placing a request with Siemens support for details, have a look at the following application note for the 6RA70 http://support.automation.siemens.com/WW/view/en/9716319. It uses free function blocks for diamter calculation. I have used this method as well as my own software in a technology module like the T400. |
Follow us on