5/29/2023 10:03 AM | |
Joined: 5/29/2023 Last visit: 6/5/2023 Posts: 3 Rating: (0) |
Hi. Good morning for everybody I have a problem with a milling machine. We make different holes in a piece and, sometime, the rpm is stop when it is making any hole and after stopping continues without stopping the machine. The problem is that the operator don´t watch the problem and this hole is not good finished. Do you Know if there are a parameter or variable to controlate RPM if is lower than 100RPM for example stop the machine ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/30/2023 04:06:22New subject after splitting |
|
5/30/2023 4:08 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Problem with RPM is published within the conference SINUMERIK CNC automation systems. Best regards, |
Follow us on