11/24/2022 12:16 PM | |
Joined: 8/26/2022 Last visit: 8/22/2024 Posts: 6 Rating: (0) |
The device I would like to use is TWN4 MultiTech 2LF NF and they have only two communication interface USB and RS 232. |
11/24/2022 12:30 PM | |
Joined: 3/30/2020 Last visit: 9/13/2024 Posts: 4756 Rating: (977) |
That company offers converters [https://www.elatec-rfid.com/en-us/tcp-converters]. It is in concept what Mr. Duris spoke of earlier which is worth taking notice of. He does have experience with cross protocol headaches. Perhaps do a proper costing. Also keep in mind the RS232 has a limit cable length. The Ethernet connection can go directly to the PLC port, though you may want a small Ethernet hub. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on