1/12/2011 3:41 AM | |
Posts: 2964 Rating: (478) |
Hi.... What is the version of Simocom U are you using it? I can able to see this parameter...Can you re check it again. Regards, Ekalavya |
1/12/2011 3:50 AM | |
Posts: 2964 Rating: (478) |
Hi.... I have connected my latop and checked i have not tried checked pressing P+ or P- Can you re-check the switch setting parameters on the 611U card Regards, Ekalavya Attachmentrs232 -rs285.pdf (1113 Downloads) |
Last edited by: Ekalavya at: 1/12/2011 4:06 AMDocument attached |
|
1/12/2011 4:53 PM | |
Posts: 50 Rating: (0) |
How did you connect your laptop first time? If the parameter is in the drive and it is set to RS485 how do you change it over to RS232? |
1/12/2011 11:17 PM | |
Posts: 50 Rating: (0) |
Anybody?? |
3/7/2016 12:07 PM | |
Joined: 12/1/2015 Last visit: 1/24/2024 Posts: 2 Rating: (0) |
Make sure you are using a pin to pin cable.
|
4/11/2018 7:25 AM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7957 Rating: (162) |
New question published by rohitbhel is split to a separate thread with the subject After formatting 611U FEPROM through software unable to communicate with that particular control card . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on