11/7/2016 10:56 PM | |
Posts: 8 Rating: (0) |
...another screenshot attached -> data block. |
11/9/2016 6:27 AM | |
Posts: 8 Rating: (0) |
Hello, Attachmentpics.pdf (89 Downloads) |
11/10/2016 8:38 AM | |
Posts: 8 Rating: (0) |
Hello I'm attaching some pictures from tests. Yesterday I connected PC to PLC and tried send the text file. It was successfully so I as sure that PLC configuration was OK. Next step was a connection to the uC [ it is not Atmega :) ] and after a few test I have realized that I'm not sending data in the right format. Now I'm sending each character separatly in hex and there are two ASCII commands 0D and 0A after character. Now my data frame is 32bytes. You can see all on the attached pictures. Thanks for the help. Regards Attachmentpics.pdf (73 Downloads) |
Follow us on