6/19/2014 12:06 PM | |
Posts: 8 Rating:
|
Hi Olloy, I have to admit that this is a last minute job thats been handed down to me, and I have no experience dealing with non-Siemens devices through profibus. I know that there are standard FBs available to send and receive but haven't used them before. I have attached the only reference documentation that I have for setting this up. The manufacturer of the hot-melt unit have today said that their interface is "a standard RS485" which is all the information that they were able to provide me other than the document I have attached. Any suggestions and information gratefully received. Matt. AttachmentPB_Xmelt_Bus2.pdf (183 Downloads) |
6/19/2014 12:42 PM | |
Joined: 12/1/2009 Last visit: 2/9/2025 Posts: 672 Rating:
|
Dear globaltech, it's not profibus you are dealing with. You will have to adapta vendor specific protocol by usingthe standard ASCII driver (send/receive function blocks) of thesiemens serial interface. Best Regards. |
Give us your feedback and show us your respect! |
|
6/19/2014 2:00 PM | |
Joined: 12/1/2009 Last visit: 2/9/2025 Posts: 672 Rating:
|
Hi olloy, the max. baudrate for CP340 is 19.2kBaud, if that Xmelt system cannot reduce the baudratehe will need to use CP341. Anyway, I believe that problemhas a lower priority now. Best Regards. |
Give us your feedback and show us your respect! |
|
This contribution was helpful to
1 thankful Users |
6/19/2014 4:40 PM | |
Joined: 1/17/2007 Last visit: 4/15/2025 Posts: 1560 Rating:
|
I very much doubt it will work. Your device is not a Profibus device and as such it will not communicate on Profibus. For the convertor to work, it would need to be a Profibus slave to RS485 convertor, with the RS485 side having the knowledge of how to get data from the XMelt using their protocol and then retransmit is over the Profibus interface. If it has the ability to do that out of the box, I would be very surprised as the XMelt protocol is unliklely to be an industry standard. Maybe the RS485 side has some programming facility such that you can program it to interface to the XMelt device. I have used similar items in the past that had a Modbus interface on one side and a free RS485 interface on the other, and it provided to simple logic to program a user defined protocol for the free RS485 side. Anybus do something that might meet your needs here:- http://www.hms.se/products/abcrs.shtml |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
This contribution was helpful to
1 thankful Users |
Follow us on