5/30/2018 10:58 PM | |
Joined: 6/5/2016 Last visit: 9/6/2024 Posts: 1 Rating: (0) |
Good day, I am not sure if I am strungling with RSTP settings between RSG2100 switch and Siprotec 4 relays. Just to give you a picture I have 5 rings of siprotec 4 relays that connect to RSG2100switch, the rings are as follows:
By default I was expecting at least 20 relays to be visible, I have no idea where does the 18 come from. I changed the RSTP settings Max Age Time from 20 to 40 and the behavior remains the same. I have also attached Netview screen short, which indicates the relays RSTP settings. On the Netview screen short what is the difference between, MaxAge-P and MaxAge-L? I have also noticed that PBDU parameter has an error on the switch, I tried ways to clear that error with no success, including reloading factory settings. I am not sure if that is the main cause of the malfunctioning. Please HELP Kind regards Ziggy Simelane ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/1/2018 11:20:59 AMNew subject after splitting |
|
Follow us on