Industry Online Support
Technical Forum
3/10/2012 3:59 PM | |
Posts: 14 Rating: (0) |
Hi Toeternietoe, Yes I have effectively connected to just three wires of the sensor by linking the two ground wires together. Yes my temperature inputs are at Ai3 & Ai4. I am begining to think the module ismaybe broken.. Cheers, Ad |
3/11/2012 11:39 AM | |
Posts: 14 Rating: (0) |
The light is green and the whole system runs on 24V DC.. 6 Module system. |
3/11/2012 12:47 PM | |
Joined: 12/27/2006 Last visit: 7/7/2024 Posts: 1197 Rating: (113) |
Post your programm here So we can look at is |
3/11/2012 11:11 PM | |
Posts: 14 Rating: (0) |
Ok please find attached both the program and a image showing it running, where you can see Ai3 & Ai4 are zero..
Attachmentsupport.zip (294 Downloads) |
3/12/2012 7:26 PM | |
Posts: 14 Rating: (0) |
Hi Helmut, I tried disconnecting and re powering but same problem.. |
Follow us on