Industry Online Support
Technical Forum
6/24/2011 9:29 AM | |
Posts: 2 Rating: (0) |
can i use s7-200 cpu 221 or cpu 222 for stepper or servo moter Run/program ? |
7/15/2011 11:59 AM | |
Posts: 45 Rating: (4) |
Hello Yes, tip #22 in the S7 200 tips section of cd #2 there is a very good description and example program howeverI needed to convert the 24v to 5v. The link below has the tip #22, down load the file. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=1232912&caller=view Have A Good Day Tom |
Last edited by: primus 1 at: 7/15/2011 12:04 PM |
|