Industry Online Support
Technical Forum
7/11/2011 1:04 PM | |
Posts: 65 Rating: (1) |
Hi, This is raghu. Actually in my case one button am using for logging the datas using VB scripts by pressing button in the HMI. But am trying to run the scipt with out pressing the button. after one cycle values has to log now it is happening by pressing the button only, i want to run the same script with out pressing the button in the HMI just by getting cycle end command from the plc, could it possible with script. My HMI is TP277 it will support scripting. Thanks and regards, Raghu Splitted from Printing WinCC Reports from PLC. |
Last edited by: O_Moderator at: 7/13/2011 11:06 AMnew subject after splitting Last edited by: raghuk at: 7/11/2011 1:06 PM |
|
7/11/2011 1:35 PM | |
Joined: 4/24/2006 Last visit: 4/19/2024 Posts: 8610 Rating: (1147)
|
Dear Raghu, Perhaps you can use the Scheduler. (see online help of WinCC flexible) Have you seen this link: how are tags and alarms logged in WinCC flexible? Best regards, Wizard |
7/11/2011 7:34 PM | |
Posts: 65 Rating: (1) |
HI Wizard, Thanks for your post. And if you have any link for WinCC Flexi scripts basics please do post. Regards, Raghu |
7/12/2011 11:56 AM | |
Joined: 4/24/2006 Last visit: 4/19/2024 Posts: 8610 Rating: (1147)
|
Dear Raghu, Perhaps the following links might help: Tips and tricks for creating scripts Which VBS information and programming aids are there in WinCC flexible? how on a Windows-based panel can you use a script to save and read out information in a text file? Or this thread: /tf/WW/en/Posts/53679 Best regards, Wizard |
Follow us on