10/21/2015 2:54 PM | |
Joined: 2/17/2014 Last visit: 5/25/2023 Posts: 1 Rating:
|
Hi there, I`m a complete stranger to the S110 drive but now I have to work with one on an indexing table. I have a S7-1214 PLC and I have to control a synchronous motor with internal holding brake with the help of a CU305 PROFINET. My question is: Can I control the position of the table (motor) with PROFIdrive? How? And if I can`t, how can i control the position of it by other means? like PTO maybe? I would like to move the table to a certain degree, and maybe send the degree I want by the PROFINET communication. Or should I control the S110 with pulses? and scale the pulses to work for degrees? How can i read the degrees from the encoder? Thank you in advance for your answer!
Cata ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/21/2015 3:42:45 PMNew subject after splitting |
|
10/21/2015 5:55 PM | |
Joined: 10/11/2006 Last visit: 6/7/2023 Posts: 5535 Rating:
|
Hello Catalin, since your questions are very generic, please have a look at the two application examples: https://support.industry.siemens.com/cs/ww/en/view/40616058 |
With best regards, |
|
Follow us on