11/7/2016 9:25 AM | |
Joined: 10/11/2006 Last visit: 5/3/2024 Posts: 5832 Rating: (790)
|
Hello, using additional DCB-Extension libraries (developed using Sinamics DCB Studio) a runtime license is required. The license can be ordered by stating the Article number 6SL3077-0AA00-0AB0 (SINAMICS DCB Extension https://support.industry.siemens.com/cs/ww/en/pv/6SL3077-0AA00-0AB0/pi) or as option U01 to CompactFlash Card. And yes, making a complete machine control without PLC is not possible, but sometimes we have costumers doing some kind of retrofitting a machine with some new equipment, where no PLC is used (e.g. using an HMI with direct access to Sinamics or just IOs). |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on