Industry Online Support
Technical Forum
1/31/2011 6:32 PM | |
Joined: 1/31/2011 Last visit: 4/27/2011 Posts: 2 Rating:
|
Hello, I want to use SINAMICS S120 (and the STARTER software) to control a rotary servo motor in speed control mode as well as intorque control. While speed control works well, I didn't manage to apply torque control. Even if I use the configuration "torque control", the control panel does not allow to set a torque value. I have read in the forum, that the STARTER software does not support such a direct torque control, but that it can be realized by using speed control and adjusting the torque limits (see /tf/WW/en/Posts/46171). But I'm a beginner and so this explanation is not sufficient for me...:-(Can anyone explain in simple words the steps needed to realize torque control? Thanks in advance! |
2/7/2011 5:55 PM | |
Joined: 1/31/2011 Last visit: 4/27/2011 Posts: 2 Rating:
|
Thanks for your advice! |
Follow us on