8/24/2021 2:51 PM | |
Joined: 2/7/2018 Last visit: 3/14/2023 Posts: 181 Rating: (30)
|
Hello, to get the 1FT2 you need to delete the 1FK2 out of the device view. Then you can insert the 1FT2 to the device with drag and drop. You can see it in two pictures i attached within the zip-folder. Best regards Technical Support for SINAMICS S210
Attachmentdraganddrop1FT2.zip (591 Downloads) |
8/31/2021 2:38 PM | |
Joined: 11/28/2019 Last visit: 7/11/2024 Posts: 3 Rating: (0) |
Hello I've been struggling with this issue for some days but still can't solve it. I managed to add 1FT2 motor according to advice of TechSupport SINAMICS S210 what is shown in s210_devview.png picture in attached .zip file. When I go to Drive parameters offline everything also seems correct (s210_param_offline.png). But when I go online it shows that no motor was configured. (s210_param_online.PNG). Moreover I can't dowload the drive with the error shown in s210_load_error.PNG picture. Nevertheless, upload is possible. But it uploads strange data shown in picture s210_devview_uploaded.PNG with which the same error in online parameters persists. And other than that, in Web view I can see the type of connected motor but with no defined parameters (s210_web.PNG) and can't perform motor commisioning - it's inactive (s210_web_commissioning.PNG). Sorry for that stream of consciousness but I feel a bit frustrated Attachments210.zip (626 Downloads) |
1/29/2022 9:13 PM | |
Joined: 3/10/2020 Last visit: 5/31/2022 Posts: 2 Rating: (0) |
a Firmware Upgrade to 5.2 Hotfix 9 has solved the Problem. |
9/4/2023 12:35 PM | |
Joined: 5/25/2021 Last visit: 11/2/2024 Posts: 25 Rating: (1) |
Any update on this ? We have the same problem |
Follow us on