6/2/2010 7:05 AM | |
Joined: 6/14/2008 Last visit: 1/25/2022 Posts: 65 Rating:
|
Hello!! EPROM of S5-110A Form is "6 ES5 910-0AA41." I cannot do German. F1 EINGABE : EINGABE EINES BAUSTEINES Which is the function which reads the contents of EPROM? I append the file which stored the screen of PG675 in the photograph. Thank you Attachmentpg675_melsec.pdf (228 Downloads) |
6/4/2010 7:03 PM | |
Joined: 6/14/2008 Last visit: 1/25/2022 Posts: 65 Rating:
|
Mr. Jim Your reply is glad. UEBERTRAGEN VON BAUSTEINEN UND DUPLIZIEREN VON DISKERREN F1 UMV : UMVERDRAHTUNG VON BAUSTEINEN
F1 START : WENN DAS AG IM STOPZUSTAND IST, WIRD NEUSTART AUSGELOEST I append the screen of PG675. Thank you Attachmentpg675 melsec 0.pdf (158 Downloads) |
6/4/2010 7:37 PM | |
Joined: 11/21/2007 Last visit: 10/3/2023 Posts: 2321 Rating:
|
Hi You can try Google Translate function to translate from German to English. http://translate.google.com/ I have tried it. It is not perfect but is able to provide reasonable translations and workable if used with some intution. Cheers Navnag |
There is no such thing as the last bug in a program |
|
6/10/2010 7:07 AM | |
Joined: 6/14/2008 Last visit: 1/25/2022 Posts: 65 Rating:
|
Hello! I tried your help. However, it does not work. Is it wrong for my procedure? Attachmentpg675_melsec_01.pdf (209 Downloads) |
6/10/2010 8:09 AM | |
Joined: 6/14/2008 Last visit: 1/25/2022 Posts: 65 Rating:
|
Hello! There was information by the thread of " S5-110A - Reading EPROM" In this thread, Sigma is said as follows. The form of the disk inserted in my PG675 is "PG675U-S0-A04." Thank you |
Follow us on