11/9/2010 4:08 AM | |
Joined: 10/7/2005 Last visit: 9/13/2024 Posts: 3020 Rating: (1054)
|
Hello Mickexzy further to Late's advise, have a look too in the startup OB's 20 & 21 ofthe S5 program and search for any STP (STOP) commands in them (the logic that "drives" the STP command will then give you further clues what to check). STS in the ISTACK is either caused by a STOP request from the program(most likely in your case)or from the PG (which we can exclude in this case) or from a SINEC L1 master(don't know is this applicable in your case,see also the 115U manual for more on this). I hope this helps |
Cheers |
|
Follow us on