7/8/2010 9:50 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, Similar like SINEC CP 1430 (from page 151th). Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
7/8/2010 8:46 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, In the FAQ: Commissioning and Configuring an ISO Transport Connection between the SIMATIC S5 and SIMATIC S7 via Industrial Ethernet http://support.automation.siemens.com/WW/view/en/17661306 You will see from the middle how such a CP is configured and how the S5 program looks like. The S5 blocks are not located in the eprom of the CPU, but are part of the S5 program. |
Best regards |
|
This contribution was helpful to2 thankful Users |
7/12/2010 11:37 AM | |
Posts: 81 Rating: (1) |
Hello, I am using COM 143 v1.1 software for CP 143 configuration where we can define the data to write and read did it lies in the CP configuration.what is STF DB editor it is with the COM software ,i wanted to know that how we can configure CP143 for the communcation to WinCC and where we can define the data to read and write from the PLC to HMI
AttachmentMy Pictures.zip (290 Downloads) |
7/20/2010 5:18 PM | |
Joined: 8/25/2005 Last visit: 6/12/2024 Posts: 1162 Rating: (110) |
Hello umair, I found the following documents: Hope they will be helpfull: CP 143 TF with NCM COM 143 TF Volume 1 of 2 CP 143 TF with NCM COM 143 TF Volume 2 of 2 Best regards Sabine |
This contribution was helpful to1 thankful Users |
Follow us on