7/19/2007 1:16 PM | |
Posts: 5822 Rating: (411) |
Hi ntban, I recommend the following Manuals: COM PROFIBUS Chapter 4. ET 200 Distributed I/O System with IM 308-C and S5-95U Chapter 5 to 8. Best regards J_Bell |
7/21/2007 4:39 AM | |
Posts: 58 Rating: (0) |
Dear J_Bell & All ! I have been read all manual that you recommend with me and some thing that I find out on the NET as GSD file, the User Guide for Profibus on Elecktronikon Combox-P manual file ... That help me to understanding alot , and I have been created myself project by Comprofibus But there are something that I can't uderstand, Please looking at the word attach file. I was working so hard but I really don't know the relation between the Input and Out put in the Profibus Slave on the Comprofibus config AND the data in the Canbus side thanks! AttachmentComProfibus_Help.zip (352 Downloads) |
7/23/2007 6:15 AM | |
Posts: 58 Rating: (0) |
Hi Late& thantzawwai Thanks for your answer,Now I will post the GSD and the Box manual thatI have. Ihave tried alot to finding something but there are nothing.That make me to reach an impasse. The bigest of my wonder is the way that data(I/O) go from Canbus side through the bridge (Combox-P) to the S5 CPU (profibus-DP side). Because this system was old , so I have not formal manual and catalog,software, config tool ...It's mean I must find all of these on the Internet .But there are nothing. Please help me more than! AttachmentGSD+Manual.zip (348 Downloads) |
Follow us on