9/17/2008 3:17 PM | |
Posts: 16 Rating: (0) |
No through the RS232 port. |
9/17/2008 3:25 PM | |
Joined: 7/15/2008 Last visit: 1/23/2024 Posts: 382 Rating: (44) |
If you add a CP 524 Card you can insert a Com Module that supports RS422. |
9/17/2008 3:55 PM | |
Posts: 16 Rating: (0) |
It's nothing that complex. This is just for testing purposes in all different aspects. I need it to communicate and recqonize different modules. |
9/17/2008 4:34 PM | ||||||
Posts: 487 Rating: (44) |
There used to be a converter from Siemens. It has a DB25 pin for RS232. So you need a DB25 to DB9 adaptorplugged at the end of it. Here is the part # and the comment from Siemens
|
|||||
9/17/2008 7:01 PM | |
Posts: 16 Rating: (0) |
Is this the cable for direct from PC to PLC or do I still need the current loop converter? |
9/17/2008 8:06 PM | |
Posts: 16 Rating: (0) |
I shall try it. Thank you everyone for your help. |
9/18/2008 2:52 AM | |
Posts: 1064 Rating: (72) |
The 6es5-734-1bd20 cable works well but you will need a 25 pin to 9 pin adapter . I have used mine with a usb to serial adapt as well with positive results |
Follow us on