11/10/2020 4:00 PM | |
Joined: 10/17/2019 Last visit: 5/1/2024 Posts: 7 Rating: (0) |
Hi. I am in process of converting a S5 program to a S7 program. My question is what decimal value the Counter C4 CV has in attached pictures? A wild guess accordning to the pictures and the attached PDF is that the decimal value is 20 depending on bit assignment found in the PDF attached. Right or Wrong? AttachmentS5 CV.zip (319 Downloads) |
11/11/2020 7:55 AM | |
Joined: 12/18/2014 Last visit: 5/2/2024 Posts: 32924 Rating: (4072) |
Which manual? And which S5 PLC?
|
11/11/2020 3:09 PM | |
Joined: 12/18/2014 Last visit: 5/2/2024 Posts: 32924 Rating: (4072) |
What du you mean with "DB H3190"? Mean you a data word in a DB with format KH and value 3190? In the attachment an extract from the manual of the S5-100U. It is similar to the S5-95U. AttachmentS5-100U Manual pages 181-185.pdf (304 Downloads) |
11/11/2020 3:17 PM | |
Joined: 12/18/2014 Last visit: 5/2/2024 Posts: 32924 Rating: (4072) |
S5 counter in STEP7 classic see attachment.
AttachmentS_CUD.pdf (312 Downloads) |
Follow us on