Industry Online Support
Technical Forum
4/30/2010 11:48 AM | |
Posts: 80 Rating: (1) |
U can solder out 3 cables from the switch terminals and put any 3 position switch. 1-N-2 |
5/10/2010 9:34 AM | |
Posts: 140 Rating: (1) |
Dear Sir, My worry is I need to seperate the two PCBs of the CPU as this is two slot CPU . Is it safe to do SO? Best regards, |
6/2/2010 6:50 PM | |
Posts: 3 Rating: (1) |
Hi, the switch is an Alco AT2S, you can separate the PCBs, but carefully. regards, Jim |
6/15/2010 8:59 AM | |
Posts: 140 Rating: (1) |
Tahnk You very .I will try to get this. |
Follow us on