9/10/2012 6:55 AM | |
Posts: 8 Rating: (0) |
Hello. I have S5-100 CPU (6ES5 100-8MA01). PLC does not go to run mode. Im setting a switch to RUN, RUN lamp will light up, but it returns to STOP immediately. May I have any advice? ISTACK is here. AttachmentSS_01.zip (183 Downloads) |
9/10/2012 7:09 AM | |
Joined: 10/7/2005 Last visit: 6/24/2024 Posts: 3008 Rating: (1052)
|
Hello Yaham Question: Do you have I/O's connected to the 100U? If not, it would explain your problem and have a look too at the FAQ S5-100U without bus module If you do have I/O modules, please give us more details about yourhardware setup 9e.g. what I/O's, RAM or EPROM card in CPU etc.)and advice what changes have been made if it has been working before etc. etc. I hope this helps |
Cheers |
|
Follow us on