6/4/2009 9:28 AM | |
Joined: 10/7/2005 Last visit: 8/8/2024 Posts: 3016 Rating: (1054) |
Hello Reid while there is nothing wrong with Siemens Step5, there is a far cheaper and admittedly more user friendly alternative S5 editor available fromIBH Softec called "S5 for Windows". You can find out more about it here: http://www.ibhsoftec-sps.de/english Another alternativeS5 editoris "PLC workshop for S5" from FasTrak (http://www.fast-soft.com) which does costs some 5 times as much as the one from IBH Softec though Ihope this helps Cheers Fritz |
Cheers |
|
This contribution was helpful to1 thankful Users |
6/5/2009 9:53 AM | |
Joined: 10/7/2005 Last visit: 8/8/2024 Posts: 3016 Rating: (1054) |
I hate to disagree withUMENCHO (as I am a big fan of his usually very helpful and informative postings), but Version 6 of IBH Softec's"S5 for Windows" does actually allow calling the Siemens S5 COM packages (under Windows 2000 and XP only), so this shouldn't be an issue against it. Having said that, I have not tried this out for myself (COM packages certainly work underSiemens's Step 5),so best to be checked with the supplier if this is a must have funtionality. Cheers Fritz |
Cheers |
|
This contribution was helpful to1 thankful Users |
6/5/2009 4:11 PM | |
Posts: 14 Rating: (0) |
Thanks everyone for all the help. I'm learning. Reid |
8/8/2024 6:51 AM | |
Joined: 7/30/2024 Last visit: 8/8/2024 Posts: 71 Rating: (1) |
New question published by hussainrai2992 is split to a separate thread with the subject Programing software for PLC S5 U95. Best regards |
Follow us on