Industry Online Support
Technical Forum
6/15/2011 9:49 PM | |
Posts: 119 Rating: (1) |
s5 time has max value 2h46m,,,,,how to put timer value more than this max value...... |
6/15/2011 10:08 PM | |
Joined: 1/28/2009 Last visit: 7/15/2024 Posts: 6844 Rating: (1364) |
you can use IEC timer like SFB3 TP (PULSE GENERATION), SFC4 TON (ON DELAY) OR SFB5 TOP (OFF DELAY).The limitation of time data type would be: from TIME#0.0h to TIME#24.855134d But, I prefer to use some home-made functions to do the task. When I want to have timing in range of hours in range 50 hours I generate a hourly pulses and just count them.Of course I consider the errors in range of minute.I can simply create the idea of 6 types of timers by programming.This is also applicable universally to all kinds of controllers in which you can not find complex function as available in STEP7. regards Attachmentsfb3.pdf (283 Downloads) |
Last edited by: hdhosseini at: 6/15/2011 10:17 PM |
|
6/25/2011 12:22 PM | |
Posts: 119 Rating: (1) |
thanks hdhosseini,your advice workes i have used SFB4 on delay timer for my program..... |
This contribution was helpful to1 thankful Users |
Follow us on