5/10/2016 9:11 AM | |
Posts: 8 Rating: (1) |
Hello Experts, I am working on S5 to S7 conversion project on which stucked on analog output scaling. In S5 following logic is written for analog output coming from S5-PID(OB251).Two analog outputs are used for Course and Find action. L DBW 96 // PID output ranging from -17980 to +17980 L 2#1111 AW SLW 4 T QW112 L DBW 96 L 2#1111111111110000 AW T QW114 My question is how to convert this in S7. How do i scale analog outputs in S7. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/10/2016 11:20:09 AMNew subject after splitting |
|
5/10/2016 11:24 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
The second thread with the subject s5 to s7 conv Analog output scaling is published within the conference SIMATIC S5 / STEP 5. Best regards
|
Follow us on