12/5/2010 9:20 AM | |
Joined: 10/7/2005 Last visit: 7/11/2024 Posts: 3009 Rating:
|
Hello Guest jklmis correctthat the manual does NOT list "B" (Block) type parameters as a permissble parameter for the "LW =" instruction. I can tell youthough that it can be used and that it was quite commonly done too in the good old S5 days. What you end up with is thenumber of the Block in accu1-LL and a (typically unused) value that represents the Block typeaccu1-LH (and accu1-H is 0). What this means in your particalur case is this (assume DB39 is used as actual parameter for "ZWDB"): LW =ZWDB// accu1 =0000 xx27 hex (I think xx is 20 hex for a DB parameter, but don't quote me on that) T FY 245 // contains value of 27 hex= 39 decimal I hope this helps |
Cheers |
|
Follow us on