Industry Online Support
Technical Forum
1/25/2009 12:02 PM | |
Posts: 103 Rating: (11) |
please help me I have big problem I have project with PLC (SIEMENS S5) & touch panel (MOLLER) my work is to replace MOLLER with SIEMENS touch panel , therefore I have to use winncc flexible , I have to transfer tags from MOLLER sw to wincc flexible 2007 but most of tags that found in MOLLER sw include (DB3 DW XX.X) when I write this tag in wincc flexible THIS TAG IS REFUSED ,in help of winccflexible he says that <In SIMATIC S5 controllers, data blocks DB0 to DB9 are reserved in the controller for the CPU, and therefore cannot be used in WinCC flexible.> in the attachment you will see picture that identify the problem please note that:I can't edit sw of PLC S5, please I needquick answer to solve this problem Attachmentwincc flexible &S5.zip (411 Downloads) |
Follow us on