12/26/2006 8:50 AM | |
Posts: 2348 Rating: (263) |
There is no problem for storing S5TIME variable in FB (also in multi). I've uploaded little project with such example - take a look at FB2. The problem might be, that you can not store TIMER variable in FB. If so - just create INT variable Timer_num. Then you can use it as SP T[#Timer_num]. Attachmentfoum_mul.zip (352 Downloads) |
12/27/2006 2:54 AM | |
Posts: 83 Rating: (1) |
Thanks Aret,Finally i found itwas only a syntax mistake! hgq |
Follow us on