4/6/2017 8:19 AM | |
Posts: 531 Rating: (34) |
Virusscanner?, firewall (domain firewall?), no Port translation, admin rights windows? |
4/6/2017 10:21 AM | |
Posts: 21 Rating: (1) |
In the file i have attached all settings. Tried windows firewall on/off with no result. I have administrative rights. Maybe i am missing settings somewhere regards kostov AttachmentDoc.pdf (44 Downloads) |
4/8/2017 2:37 PM | |
Posts: 21 Rating: (1) |
Hi again I restored default settings of M874 and did the settings again. Also i had to disable WIFI adapter on the laptop in order to be able to ping M874 (192.168.2.1) and the S7-1500 (192.168.2.3) which is behind M874. I am also able to enter in the 1500's web server via browser. But my biggest goal is to be able to program the PLC with TIA Portal trough the very same PC (the Siemens application example states i would be able). When i search for accessible devices with the TIA Portal i wouldn't find the PLC. It only finds S612 but nothing beyond. Am i missing something? Do i have to use SSC for that purpose or something else.? or within 1500 settings to be visible? Regards Kostov AttachmentBinder1.pdf (41 Downloads) |
Last edited by: Pavel Kostov at: 4/10/2017 10:59:32 AMLast edited by: Pavel Kostov at: 4/10/2017 12:16:32 PM |
|
4/11/2017 8:41 AM | |
Posts: 21 Rating: (1) |
I wonder if anyone have made such connection Setting up a secure VPN Connection between SCALANCE S and M874 Using a static IP Address and successfully connected TIA Portal with the accessible devises behind M874-3? Regards Kostov |
Follow us on