12/9/2013 8:14 AM | |
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating:
|
I dont think so there will be requirement of other additional card/module. Can u mention which S7-1200 CPU u r using? |
12/9/2013 11:21 AM | |
Posts: 4 Rating:
|
Hi, The CPU i am using in this project is 1214C..
|
12/11/2013 2:16 PM | |
Joined: 3/20/2013 Last visit: 4/16/2025 Posts: 676 Rating:
|
hey! to speak to your modbus tcp device with the plc (cpu 1214c) you can use the modbus-instructions of this cpu. they are called MB_CLIENT and MB_SERVER. Some hints to this topic can you find in the forum like here and here. here is an FAQ for the VARIANT datatype. You can find more topics to the MB_CLIENT and MB_SERVER in the forum and in the online help. |
Best Regards, |
|
12/13/2013 9:55 AM | |
Joined: 3/20/2013 Last visit: 4/16/2025 Posts: 676 Rating:
|
There is Modbus RTU (RS485) and Modbus TCP (Ethernet) . Perhaps have a short look about that in wikipedia, or sth. else. |
Best Regards, |
|
Follow us on